STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Insufficient document of BL462E-CELL1

Hi!I have bought BL462E-Cell1. I need the documents of Murata Type1SC which is the key component of the discovery kit BL462E-Cell1. From the registration code printed on the sheet with BL462E-cell cannot give me the access to the documents of Murata...

ZWH.1 by Associate II
  • 3007 Views
  • 5 replies
  • 1 kudos

Resolved! Programming a SWD connection to external ST-LINK/V2

Hello. I use the NUCLEO-G071RB together with the STM32CubeIDE (Ver. 1.14.0) and STM32CubeMX (Ver. 6.10.0). I completed the first prototype phase and ported the code to a custom board with a STM32G0 MCU.I used an external ST-LINK/V2 debugger to write ...

Kmax18 by Senior II
  • 7177 Views
  • 3 replies
  • 1 kudos

Resolved! Erasing flash during RTOS task execution on STM32F4

Hi .. I am using this function to erase some sectors on the flash bool FLASH_EraseSectors(uint32_t starting_sector , uint8_t number_of_sectors) { FLASH_EraseInitTypeDef erase_init; uint32_t page_error;   /* Erase the user Flash area */ erase_...

SGasp.1 by Senior
  • 14382 Views
  • 31 replies
  • 0 kudos

STM32F411 OpenBootloader

Hi, Is there an example of an open bootloader for the STM32F4xx series? I've attempted to adapt an open bootloader example from the STM32C0xx series to create an example for the STM32F411, but I'm encountering numerous errors due to differences in th...

Mabou.1 by Associate II
  • 1756 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.