STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F303C6T6 ADC DUAL REGULAR MODE

Hello, I am experiencing a problem with ADC1 and ADC2. I configured them in Dual Regular Simultaneous Mode, where ADC1 acts as the master and ADC2 acts as the slave. The ADC channel connections are as follows: ADC1 Channel 1: 24V_Sense ADC1 Channel...

Resolved! FMAC Cascade for SOS

Hi Together,I am currently trying to use the FMAC hardware accelerator. Normal usage already works. Now for numerical stability I want to implement the filter as second order sections (sos). According to RM0481:Cascaded filters must either be combine...

Resolved! Timer1 Interrupt is not generated

I am using Nucleo-F446RE board and trying to verify the TIM1 update interrupt and PWM, the PWM is generated but if i put a break point in the update interrupt it does not halt, what is the reason?int main(void) { /* USER CODE BEGIN 1 */ /* USER...

STuser2 by Senior III
  • 546 Views
  • 5 replies
  • 3 kudos

Resolved! STM32C071 USB stack

I just started looking at the STM32C071 family as an alternative to the STM32F042 and STM32F072 we currently use. To my disappointment the USB stack for the C071 is a total mess (dozens of files and complete spaghetti) and on top of that it seems to ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.