STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F103 Multiple wakeup sources detection. Unable to read RTC_CRL[ALRF] flag after reset from STBY

Hello,In this thread, I would like to clarify a point regarding how to read the RTC_CLR[ALRF] flag. I am using the STM32F103C8T6 microcontroller and the STM32Cube Firmware (HAL) version 1.8.5. This flag indicates that the alarm has been activated.My ...

Cgelectronics_2-1695502691819.png Cgelectronics_0-1695500851362.png Cgelectronics_1-1695501377490.png

Need Assistance with PDM2PCM on STM32F407-DISC1

Hello, I am using an open source voice-recognition software known as Picovoice. To use their library it must be passed a PCM signal at a certain rate with a specific number of samples per frame. I used CubeMX to enable the PDM2PCM library on the STM3...

GSkoumal by Associate II
  • 1263 Views
  • 0 replies
  • 0 kudos

USB CDC flushing TX buffer

Posted on September 18, 2017 at 15:52A brief introduction to this problem:STM32F7 is configured for USB Device FS. USB interface is used to transmit a large array of data from MCU to computer. If, by any chance user closes the Virtual Com Port of MC...

Resolved! ADC "volatile uint16_t" data

I am using STM32F407G.I am attaching a main.c (that use DMA) that reads simultaneously the voltage coming from 3 potentiometers connected to 3 channels of ADC.In the code, if you try to change "volatile uint16_t adc_value[3]" to "volatile uint32_t ad...

errore.png
luke514 by Senior
  • 3395 Views
  • 3 replies
  • 1 kudos

Resolved! USBPD Library missing usbpd_lowpower.h

 Hello,I am using the STM32 USBPD Library in a DRP battery bank application, and want to reduce idle power consumption. In the documentation and source files, there is mention of a usbpd_lowpower.h file but I cannot find this file anywhere.There is a...

NMartin by Associate III
  • 1902 Views
  • 3 replies
  • 1 kudos

Resolved! Seeking Assistance with Variable-Length UART Receive Interrupts on STM32F091RC using STM32Cube IDE

Dear ST Community,I'm currently working on STM32F091RC using STM32Cube IDE, and I've encountered an issue with handling UART receive interrupts for variable-length data. Currently, I have set a fixed length of 5 bytes for the data, and the UART commu...

SANTHOSH1 by Associate II
  • 3569 Views
  • 5 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.