STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VCP problem Linux/Haswell

Posted on May 21, 2014 at 09:28Hello, sorry for off-topic. Has somebody experienced problems with VCP in Linux with Z87/H87 chipsets? I have some fail-reports from clients and also tried it on colleagues computer. After several working sessions with...

mastykin by Associate II
  • 1479 Views
  • 2 replies
  • 0 kudos

USB to USB Protocol Converter - STM32F2

Posted on January 17, 2014 at 03:21I have an legacy uninterruptible power supply (UPS) that communicates to a host over USB.  The commands are proprietary.  The UPS is now obsolete and will be replaced with a new UPS. The new UPS still connects to t...

spencer2 by Associate
  • 1214 Views
  • 2 replies
  • 0 kudos

Help transfering data to PC

Posted on December 12, 2011 at 08:47Hello there, I desperatly need help getting data from my stm32f4 to my pc. I was thinking of using the OTG and set it up as a keyboard and transfer the data accross like that but it seems like a huge mission to tr...

pumzele by Associate II
  • 11893 Views
  • 26 replies
  • 0 kudos

STM32f407 Dsicovery - USB Communication

Posted on June 12, 2012 at 12:59I am a beginner in the ARM cortex series and so far have successfully managed to program basics like GPIOs ADCs DACs TIMs . Part of my project requires me to transfer all processed data to the PC using USB communicati...

USB CDC, composite device, Windows SetupAPI

Posted on May 12, 2014 at 12:15Hello, I tried virtual COM port example on STM32 and used driver VCP_V1.3.1. I'm surprised that without pre-installing driver the device is found as a composite in Device Manager, and I cannot use the same inf file (at...

mastykin by Associate II
  • 8554 Views
  • 15 replies
  • 0 kudos

How to connect STM32F103 to PC with USB

Posted on May 14, 2014 at 16:34Hi, as you know some basic STM32 microcontrollers has a USB connector. (USBDM,USBDP)Now, I wanna OV7670 camera is connected via a USB connection to the PC, and I'd an image to the PC (e.g. MATLAB programs). How can con...

mrezakhd by Associate
  • 864 Views
  • 0 replies
  • 0 kudos

Using LWIP to communicate with PC

Posted on May 12, 2014 at 18:27Hi everybody,is there somebody who can explain me on a short example how I can use the LWIP TCP/ IP Protocoll to read and write data by myself. I tried it for a while and used google but i can't find the right solution...

breibold by Associate II
  • 742 Views
  • 0 replies
  • 0 kudos

FATFS LONGFILE NAME SETTING

Posted on May 09, 2014 at 06:55PLZ HELP ME OUT HOW TO ENABLE LONG FILE NAME FORMAT WHEN USING FATFS LIB FOR 4 GB SD CARD #lfn #fatfs #fatffs-long-file-name

soobia by Associate II
  • 1590 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.