STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4-Discovery ADC problem using HAL driver

Posted on January 17, 2015 at 18:54Hi,I'm using HAL driver to configure ADC module.  This is my code:void adc_config(){   AdcHandle.Instance = ADC1;   __ADC1_CLK_ENABLE();   HAL_ADC_DeInit(&AdcHandle);   AdcHandle.Init.ClockPrescaler = ADC_CLOCK...

zivadin by Associate II
  • 1880 Views
  • 1 replies
  • 1 kudos

DfuSe redistribution terms?

Posted on June 06, 2014 at 18:45Hi, I need to provide the end-user with a customized way to flash the firmware to our product. What are the redistribution terms on the DFU driver, STDFU.dll and the binary code compiled using the provided sources? Th...

stano by Associate
  • 1605 Views
  • 4 replies
  • 0 kudos

Compiling programs that will be bootloaded

Posted on January 15, 2015 at 18:53These forums are great, thanks in advance for all your help!I'm using an STM32F439, no IDE has been picked yet, but either Keil or IARMy application involves swappable FLASH (or EEPROM) boards that contain the prog...

STM32Cube DSP libraries

Posted on March 21, 2014 at 17:56Does anyone know what happened to the DSP libraries? I'm trying to get some arm_... basic math functions to work with the new HAL libraries used by STM32Cube and the header files used in the CMSIS/DSP_lib library won...

vlad by Associate
  • 3095 Views
  • 8 replies
  • 0 kudos

STM32F205 close USB HW complitly

Posted on January 13, 2015 at 13:09I have an application which use the USB in the Boot but close it when I move to the APP. On the APP I stay on the stop mode. I notice I have extra 0.5ma there. When I didn't active the USB at all in the Boot I get ...

Barbie by Associate II
  • 1182 Views
  • 1 replies
  • 0 kudos

Using STM32 Cube with Raisonance Ride7

Posted on January 14, 2015 at 17:44An application note AN0063 describing how to use the STM32 Cube with the Raisonance Ride7 software development environment is available on the support web site for the Raisonance tools:  http://support-raisonance...

lwip on E407 board, source for STs AN3966

Posted on January 13, 2015 at 23:40Hi all, I want to run lwip on the Olimex E407 board. STs AN3966 seems to be a good start, but I cannnot find the ST modifications auf the software. It is not in the download from http://savannah.nongnu.org/projects...

detlef by Associate
  • 1783 Views
  • 2 replies
  • 0 kudos

STM32F105 eeprom simulation

Posted on January 13, 2015 at 10:27 Hello I am try write a configuration in a microcontroller STM32F I am using stsw-stm32010 code base example. The example work properly. But when I make my code don't work. I want...

lemac by Associate III
  • 1197 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.