STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL driver CAN msg typedefs

Posted on October 16, 2015 at 19:24 I worked a lot with the StandardPeriphLib but now I try to migrate over to the HAL driver for new projects. The HAL driver come with a heavy overhead. For example, without any optimization level the function H...

op by Associate
  • 2151 Views
  • 5 replies
  • 0 kudos

STM32F030C6 Entering Bootloader of Virgin Device

Posted on August 06, 2015 at 16:46In the STM32F0 reference manual it states that only the STM32F070x6 and STM32F030xC devices support the empty check for entering the bootloader on virgin devices. Is any way to enter the bootloader on the STM32F030C...

tderensis by Associate II
  • 1567 Views
  • 3 replies
  • 0 kudos

Generic HID on STM32L053

Posted on October 16, 2015 at 11:37We are using STM32L053 in our project. We evaluated the USB data transfer using CDC(Virtual COM port) and USB composite device. However, both of them require specific ST drivers for the PC to recognize the USB devi...

aravinda by Associate II
  • 2083 Views
  • 6 replies
  • 0 kudos

USB not working putting the CPU in low power

Posted on October 16, 2015 at 13:39Hi all I've been using the STM32F429 discovery board since a long time with optimal resultsI've been using USB HID device profile successfully for long time.Now I'm trying to put CPU in low power mode (the first ty...

damiano2 by Associate
  • 756 Views
  • 0 replies
  • 0 kudos

STM32F4 Discovery - merge two USB descriptors

Posted on October 16, 2015 at 12:20Dear all, I'm using STM32F4 Discovery board and I wrote two separate projects: Audio USB Device (that uses Audio class USB descriptor)General purpose Device (that uses CDC USB descriptor)How can I merge these tw...

aressia by Associate II
  • 575 Views
  • 0 replies
  • 0 kudos

Problem identification USB CDC Device

Posted on October 13, 2015 at 15:15Hi, I'm using STM32f407 for a USB project. I use CDC class (STM32_USB_Device_Library) for implementing USB device on my OLIMEX EVAL board. When I connect my board to PC, it appear as VCP, as shown in the figure att...

vlr by Associate II
  • 2038 Views
  • 2 replies
  • 0 kudos

Problem with file startup_stm32f407xx.S

Posted on October 14, 2015 at 16:37Hi, i'm using STM32f407 for a USB project. I use CDC class (STM32_USB_Device_Library) for implementing USB device on my OLIMEX EVAL board. When i connect my board to PC, it appear as VCP, but device manager says: ...

vlr by Associate II
  • 1467 Views
  • 1 replies
  • 0 kudos

Info USB CDC Device Descriptor

Posted on October 06, 2015 at 16:24Hi, I'm using STM32f407 for a USB project. I use CDC class for implementing USB device on my OLIMEX EVAL board. This is my Device Descriptor: __ALIGN_BEGIN uint8_t USBD_DeviceDesc[USB_LEN_DEV_DESC] __ALIGN_END = ...

vlr by Associate II
  • 1192 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.