STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F40G-EVAL Ethernet Lwip IAP application

Posted on October 30, 2015 at 20:20Hello, I am trying to implement the LWIP_IAP application on the STM32f40g EVAL board. After compiling the project, the program size turns out to be as follows. Program Size: Code=28150 RO-data=3114 RW-data=260 ZI-d...

bhatia by Associate
  • 1371 Views
  • 1 replies
  • 0 kudos

Cortex m0+ eeprom

Posted on October 30, 2015 at 15:55Hello, I use a Cortex M0 + to develop an application. With this cortex, I need to write in memory and this take 12 seconds by bytes. Could someone tell me if this is normal or not? thanks in advance . I'm using...

SDIO vs SPI

Posted on December 09, 2013 at 17:03I am using STM32f4 ,fat fs & SPI mode to interface to SD card every thing works fine .but i want to use DMA to increase read performance.should i go for SDIO to achieve a little more speed or is there any way to t...

STM32 Composite Device (MSC+CDC)

Posted on October 15, 2015 at 14:46 I suffered a week and wrote all the same USB Composite device (MSC+CDC). The point is this: I wrote Composite device MSC CDC. Everything is determined by the Manager, MSC works on both transmit and receive,...

thefoxek by Associate II
  • 1239 Views
  • 1 replies
  • 0 kudos

STm32F USB VCP example

Posted on March 10, 2015 at 16:12 I am building a microcontroller based on the STM32F302K8 chip and I am trying to send data to host PC via USB. My echo code below based on an example in the forums works: static int8_t CDC_Receive_FS ...

B Zikhali by Associate III
  • 4842 Views
  • 11 replies
  • 0 kudos

View Trace with Eclipse

Posted on October 29, 2015 at 10:28 Hi, I'm new to STM32 and I got a STM32F7 Discovery Board. I'm playing around with the USB Host MSC Standalone Application example provided in the STM32Cube_FW_F7 package. In the Application, th...

merelda by Associate
  • 784 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.