STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L476 power up issue

Posted on May 31, 2018 at 08:26I have built a custom board and I have used the reference design provided with NUCLEO-L476RG. When I apply power to the board it doesn't power up. I have to connect VCC form powe supply on board and connect NRST on boa...

System Bootloader vs. IAP - risk assessment

Posted on May 30, 2018 at 18:24Hey folks,I'm developing a system using the STM32F407 for an application where hardware malfunctions and especially corruption of flash memory due to environmental influences is a thing.Additionally, the system works i...

CubeF0 ADC LL bug

Posted on August 24, 2017 at 13:24LL_ADC_Init in CubeF0 contains a check for ADC_InitStruct.Clock, which is not used in the function. CubeMX does not generate a value for ADC_InitStruct.Clock and thus the assert in LL_ADC_Init fails.ADC_InitStruct.C...

Resolved! USB Host Interrupt OUT

Posted on May 15, 2018 at 01:08 STM32L4xx HAL 1.11 Framework Modifying the ST USB Host library to include the missing states in the static USBH_StatusTypeDef USBH_HID_Process(USBH_HandleTypeDef *phost)�?�? method that runs the HID Cla...

0690X0000060KigQAE.png

Resolved! STM32F107 IN TCP CLIENT MODE

Posted on May 28, 2018 at 05:54hello!      According to my experience, STM-controller is one of the best controllers I have ever worked with. currently, I'm working on a project based on STM32F103ZET6 controller and everything works really fine and ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.