STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo-F746GZ CDC not enumerating

Using CubeMX I generated a project that uses just the USB Device and CDC middleware. It builds without errors, however when plugged into Windows PC it fails to enumerate. The error shown is "A request for the USB BOS descriptor failed." I hope someon...

Error connecting to com port on composite cdc+msc

Hi everyone,i have an issue i can't connect to my com port using a composite device project.In the device manager everything is fine and the mcu is displaying as 2 devices but somehow i can't connect to the com port with any terminal program.I attach...

arduo by Senior
  • 581 Views
  • 0 replies
  • 0 kudos

I2C Driver STM32f469

After initialisation thru latest CubeMx I2C using LL_Driver, I found few functions missing in stm32f4xx_ll_i2c.h, ie. (LL_I2C_HandleTransfer).I did refer few examples for some F0 device but could make out anything useful.Please provide me some soluti...

Abhi1 by Associate II
  • 1661 Views
  • 3 replies
  • 0 kudos

Problem with CAN on STM32F091 uC

Dear all, I'm currently trying to work around the CAN Bus on the STM32F091CB uC, with StdPeriph_Lib_V1.5.0 Lib but the transmission is never successful (I have already programmed STM32F4 and STM32F7 boards with StdPeriph_Libs, without any problem).Th...

AGraj by Associate
  • 899 Views
  • 0 replies
  • 0 kudos

How Erase Flash memory with stm32h750VB?

Hi everyone, My project consist, in a bootloader with USB MSC, and the size of flash of this uC is 128k bytes, that is, there is only one sector.I had some problems with bootloader of this uC. If i program first time, all right, but if i program sec...

I2C not working on STM32L053R8T6 ?

I have added the code written in HAL for I2C communication between I2C 2 of STM32L053R8T6 and LIs3dh accelerometer to receive whoami register. doesn't seem to be able to receive any data from the accelerometer.#include "stm32l0xx.h"#include "stm32l0x...

ASING.91 by Associate II
  • 4902 Views
  • 12 replies
  • 0 kudos

Why does the built-in SPI-bootloader in STM32F446 fails to write to flash address 0x0802ADF8, when all the previous addresses were written to just fine?

I have an STM32F446 that has its firmware upgraded by another microcontroller through SPI-bus (please see AN4286, "SPI protocol used in the STM32 bootloader"). My application code starts at sector 4 (address 0x08010000) and I am able to successfully ...

arnold_w by Senior II
  • 893 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.