STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CDC Device descriptior request failed

I want to realize CDC function to transimit/receive data to/from PC via STM32F105RB. I get the code from Cube. Set clock, enable CDC and modify heap size to 0x1000. But when I power on deivce, "Device descriptior request failed" shown.1.I don't know ...

Creating spi shift register

is it possible to create spi shift register on the slaves.for example, the master sends 200 bytes. the slaves keeps shiftting bytes until the NSS goes high. kindly advise how can this be implemented?Thanks

AOmar by Associate II
  • 445 Views
  • 0 replies
  • 0 kudos

USB ID pin interrupt

GPIO configuration as followsvoid HAL_HCD_MspInit(HCD_HandleTypeDef *hhcd){...  GPIO_InitStruct.Pin = GPIO_PIN_10;  GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;  GPIO_InitStruct.Pull = GPIO_PULLUP;  GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;  GPIO_InitStruc...

YChun.5 by Associate
  • 722 Views
  • 0 replies
  • 0 kudos

stm32f7 + freertos +USBFS MSC stack not working

I am starting to use stm32f7 + freertos +USBFS MSC stack in the produce, but never work. I start from CubeMX, and it works if no freeRtos. The file can be written and opened without a problem, but with the FreeRtos, the code always stuck in the file-...

kqian by Associate II
  • 780 Views
  • 0 replies
  • 0 kudos

Bootloader and distance reprogramming

Hello,I program on the NUCLEO-144 STM32F767ZI board and I have been facing a problem for over a week.In FLASH memory, I have 3 programs located at specific addresses:- A bootloader which allows to start on the main programmer or reprogramming program...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.