STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I use dp83848 for stm32h7?

Hi ,I made ethernet communication with lan8742a phy driver on stm32h743zi but I have to use dp83848 and cubemx doesn't support dp83848 for stm32h7.Is there anyone who can help ?

Bilge by Associate III
  • 1205 Views
  • 1 replies
  • 0 kudos

STM32F777: Strange NETCONN behavior?

Hello!There are two FreeRTOS tasks, each of which creates its own NETCONN object. In one task (the first one begins to execute) there are no oddities when creating a NETCONN object. And in the second task there is: the object returned by netconn_new ...

0690X00000AQuwwQAD.png 0690X00000AQuxLQAT.png
Dimonira by Associate II
  • 730 Views
  • 0 replies
  • 0 kudos

Firmware upgrade problem

How to make DFU jump to a location from where the Factory USB DFU of STM32F070xx resides and it takes control from there? This task is to be achieved using application code instead of the hardware method to pull BOOT0 pin low.We are able to do the Fi...

Resolved! LL drivers PLL initialization

Hi all,I am experiencing some problem with PLL initialization using LL drivers.The code I am using for HSE, PLL and SYS clock is the following:void init_RCC_HSE(void) { //LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOH);   LL_RCC_HSE_Enable(); ...

simo zz by Senior II
  • 1995 Views
  • 4 replies
  • 0 kudos

Resolved! USB Video Class device on L4 HAL library

Hello,I'm working on a DCMI to USB Video Class Device converter for a project of my organization. The image sensor is a ultra low power custom design grayscale level with 640x480 resolution (8 bit per pixel). The DCMI acquisition is working and now I...

STM32H743 TCP-IP fault (FreeRTOS LwIP)

Hi all!I'm trying to use LwIP stack on STM32H743XI.I am installing a TCP-IP server. I use CubeMX for initialization. The ethernetif.c file is slightly edited to temporarily disable the d-cache in one of the I / O functions, as shown in one issue, thi...

MKise by Associate
  • 1793 Views
  • 0 replies
  • 1 kudos

How to get SDIO+FreeRTOS working on STM32F429Z ?

Hello,STM32F429Z to implement SDIO 1 bit using FreeRTOS,tried numerous examples but had no luck.1. Works fine without RTOS 2. Doesn't work with RTOS+DMA in either of the SDIO modes 3. Would like to know the cubeMX.ioc file configuration/setupNOTE - C...

NikhilAG by Associate
  • 835 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.