STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC common registers inaccessible?

Hello,i have a problem. I cant write any values into ADC12 common configuration register CCR. It is not possible if ADCs are disabled (as recomended in ref.man.) either they are enabled. I tried to change it using LL functions or CMSIS registers acce...

JCtib by Associate II
  • 1213 Views
  • 4 replies
  • 0 kudos

Resolved! CubeMx generated code for STM32h7 when QuadSPi enabled but sd card disabled not compiling (perhaps bug in generated code)

When I generate code for the STM32h750 via cubeMX, I see in stm32h7xx_ll_delayblock.h:#if defined(HAL_SD_MODULE_ENABLED) || defined(HAL_QSPI_MODULE_ENABLED)I have QSPI enabled, but SD disabled, and the code following the #if is accounted for in the c...

RMart.0 by Associate III
  • 1703 Views
  • 3 replies
  • 0 kudos

stm32 f107 i2s and sd card via dma

void DMA1_Channel5_IRQHandler() { if(DMA_GetFlagStatus(DMA1_FLAG_TC5)) { transfer_complete_flag=1; DMA_ClearFlag(DMA1_FLAG_TC5); } if(DMA_GetFlagStatus(DMA1_FLAG_HT5)) { ht_c=1; DMA_ClearFlag(DMA1_FLAG_HT5); } } int counter=0; ...

Amal by Associate III
  • 2089 Views
  • 4 replies
  • 1 kudos

STM32F072 USB Firmware Update

I am using an STM32F072 MCU in my project and in the development phase, things seem to be working properly. The boot0 pin is pulled low and I can upload firmware via the ST-LINK debugger. When the product is released to the costumer, there are two po...

AHuss.2 by Associate
  • 1581 Views
  • 1 replies
  • 0 kudos

STM32f3 STD lib ADC init problem

Hello everyone.I have problem with ADC module of STM32F3. I have two board, one board use STM32F334K8T6 is the first version of my prototype, one board use STM32F334C8T6 is new version. I have use ADC module in my program and using STD lib. but with ...

thang le by Associate
  • 1189 Views
  • 1 replies
  • 1 kudos

Troubles with FreeRTOS-HardFaults-Mallocs etc

Hello all,i'm facing a lot of troubles to run my server application on stm32.The server runs in a task. I'm using FreeRTOS. I can't explain everything here but i can share the code.First of all my application goes into HardFault in a kinda random way...

AGaru by Associate III
  • 3681 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.