STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am not able to communicate on Virtual COM port. If I am using Both functionality(receiving and transmitting). I am using STM32F103C8 MCU.

It is showing me Error "USB is unrecognized". Only Transmitting Function is working Properly.int8_t CDC_Receive_FS_User (uint8_t* Buf, uint32_t *Len)//Non-Static { CDC_Receive_FS(Buf,Len);// >> static Funcation( usbd_cdc_if.c ) } /* * if I am NOT...

Resolved! Using USB hub with STM32F7 USB HS

Hello,I'm designing an embedded system that connects to a PC for USB data and converts it to an analog signal.This is an HS USB device with 2 USB ports which needs to process 4 channel 40Mbps data.This device can work as a single system, but with som...

0690X00000BvotTQAR.png
BHan.1 by Associate II
  • 3945 Views
  • 12 replies
  • 0 kudos

Resolved! Whats the use of System memory & flash memory

Please any one help how to differentiate the system memory & flash memory in STM32MCUs, Whats the use of the both memory?Where we need to store the user code & where we need to store the customized setting?How to store FAT(File Allocation Table)?How ...

Sprak.11 by Associate II
  • 5616 Views
  • 2 replies
  • 0 kudos

Resolved! Locate the STM32F405RGT6 HAL_User_Manual

I cannot find the ??-> STM32F405Rx_User_Manual <-?? in the STM32F4xx_HAL_Driver package in the STM32Cube_FW_F4_V1.24.2 in my repository. Is it available? Also I would like one for the STM32F4 Discovery's 407VGT6 MCU as well, but the 405RGT6 would suf...

JSmit.22 by Associate
  • 1417 Views
  • 2 replies
  • 0 kudos

Can STM32 set it self to bootloader mode thru software

I am trying to get STM32 to set it self bootloader mode.One processor that I am trying to do it with is stm32f070rb and the second is stm32f070x6.I send command to each of them, and in their program I set RX Callback to handle this command.here is ex...

0690X00000BvqOcQAJ.jpg 0690X00000BvqOwQAJ.jpg 0690X00000BvqPGQAZ.jpg
DKubi by Associate II
  • 2864 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.