STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32Cube : FATFS and exFAT

Hi,I have worked on STM32F722VE MCU with FATFS with USB MSD , SDCard.Will is possible to Enable FATFS with exFAT with STMCube Generated Code and used both File format simultaneously in Storage Devices ?For SPI Card/SDMCC SD Card/USB MSB Thumb Drive ...

0690X00000DA2QSQA1.png

Am using Windows 7 Ultimate , x86. Also tried a separate Linux Ubuntu 18.04.3 PC , with same result. Can't get Virtual COM Port to enumerate using STSW-STM32102 USB driver installation package. Get, "device descriptor read/64, error -71" reported.

Does anyone know how to edit the device descriptor when using this driver package and can explain this in detail ? The uC is a STM32L082KZT6. The Virtual COM Port (VID 0483 PID 5740) is a USB CDC class 2 device. The associated USB DFU (VID 0483 PID D...

Resolved! Ethernet example for STM32H745I-DISCO

Hi All,I have a ST32H745I-DISCO and would like to use its Ethernet port. It has a LAN8740A PHY connected to the MII port. There seems to be no Ethernet example for the STM32H745I-DISCO in stm32cubeh7. Does anyone know of an example that uses STM32 ...

Ade1 by Associate II
  • 1909 Views
  • 2 replies
  • 0 kudos

I want to send data from my Nucleo board to Matlab using the USB interface with the CDC protocol. But I am not able to open the port. What can I do to use the virtual COM port?

Request for help with USB CDC interface(STM32F401 Can not open Virtual Port)I want to send data at about 5Mbit/s from my Nucleo board to Matlab using the USB interface with the CDC protocol. I have now managed to get the PC to recognize a "Serial USB...

MScha.1 by Associate II
  • 1037 Views
  • 0 replies
  • 0 kudos

USB not working on STM32F302C8 board

We are developing a USB prototype based around STM32F302C8. I cannot get this device to enumerate on USB, using either my own firmware, or the ST examples in STM32Cube_FW_F3_V1.11.0\Projects\STM32F302R8-Nucleo\Applications\USB_DeviceThere is some act...

PMcNe.1 by Associate
  • 691 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.