STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 USB Mass Storage Host with Black Board

Hello There,I am implementing USB Mass storage host on STM32f407ve board. The board which I am users is STM32F4 Blackboard Image and schematics attached. Appli_state always remains Idle. I tried removed resister 21 but still not able to create file i...

Junaid by Associate II
  • 2360 Views
  • 0 replies
  • 0 kudos

Stm32 hid touch

Hi, I'm struggling converting hid mouse to hid touch controller. I'm using discover board stm32f411. There are 2 problems that I'm struggling are1. My code only sending 4 bytes of data to host2. The maxim x,y data only 127Can anyone help me? Thanks​

Bnguy.11 by Associate
  • 803 Views
  • 0 replies
  • 0 kudos

STM32F0 USB CDC not working with Windows 7

Hi all,I have a custom board made with STM32F070C6T6. I tried to implement USB CDC, and everything works fine on Windows 10 but in Windows 7 I cannot open the serial port although the Device Manager recognize it and the device status says "This devi...

vtran1 by Associate II
  • 1289 Views
  • 1 replies
  • 0 kudos

general stm32f41x usb endpoint settings

i'm using the stm32f411CEU6. I build the USB composite device. running MSC+CDC, works, but when add the HID, mean MSC+CDC+HID, it doesn't work. seems the endpoint issue. and when only use the HID+MSC, also doesn't work. with the old HAL version when ...

cchao by Associate II
  • 703 Views
  • 0 replies
  • 0 kudos

Nucleo-144 STM32F746, FreeRTOS, LWIP

Hello,I have a problem with LWIP. LWIP doesn’t property work on Nucleo-144 STM32F746 with default settings. After three ping telegrams  LWIP doesn’t work anymore and  FreeRTOS tasks are blocked.DHCP is activated and I get IP dynamically from DHCP-Ser...

Isol by Associate II
  • 2356 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.