STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Use USB Peripheral as UART with STM32L4.

Hi,I'm currently developing a board where I use STM32L433RC as my main unitof processment. This board will have an SD Card to store some data and later ontransfer it via UART. To achieve this, I must use an UART to Serial Portconverter.After some res...

MAndr.233 by Associate III
  • 5678 Views
  • 4 replies
  • 0 kudos

Using WriteMemory command of STM32L45xxx bootloader

Hi,Iam trying to write some data (i.e. 8 bytes) via the WriteMemory command of STM32L45xxx bootloader to the STM32's SRAM area (in particular to address 0x20000000). However when I connect to the device and look into the memory the data is not take...

SKrey.1 by Associate II
  • 1445 Views
  • 2 replies
  • 0 kudos

I have a question about hid otg connector selection

I am trying to implement hid otg with stm32f105But you can use micro 5pin as otg usb connectorUSB communication does not work with the normal connector as shown in the picture below.I wonder why it doesn't work depending on the usb connectorAnd is th...

0693W000001cOPjQAM.jpg
HSHIN.1 by Associate
  • 1535 Views
  • 3 replies
  • 0 kudos

STM32 USB Data Logger

Which Software you are using to monitor the Receive and transmit data from USB. Do you have any suggestions for the USB data Loggers ?

Smalik by Associate II
  • 761 Views
  • 0 replies
  • 0 kudos

USB Audio issues with repeat INCOMPISOOUT interrupt

I'm having trouble implementing the Audio Device Class example from the STM32CubeMX tool on a STM32H750VBT6. When run, the USB appears to enumerate properly, installs the default drivers (Windows 7, btw) and shows up properly as a playback device. Ho...

YDong.11 by Associate II
  • 971 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.