STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo l152RE virtual com port not work

I have my Nucleo l152RE board i want send and receive small data using vpc , then i use cdc configuration then my program : MX_GPIO_Init(); MX_USART2_UART_Init(); MX_USB_DEVICE_Init(); /* USER CODE BEGIN 2 */ /* USER CODE END 2 */ /* Infinite loop */...

bfran.1 by Associate II
  • 2315 Views
  • 1 replies
  • 0 kudos

USB CDC Class Doesn't work

I Developed a hardware USB HS Application with STM32H750+USB3300​, and just run the softerware generated by CubeMX. I make sure that the device is enumed successful by capturing the packets with wireshark. but it still show me an fail icon(an yellow ...

0693W000003BlByQAK.bmp 0693W000003BlCNQA0.bmp 0693W000003BlCXQA0.bmp
YKs by Associate
  • 2825 Views
  • 2 replies
  • 1 kudos

STM32F746 In-circuit Flash writing problem

HiI am using the Nucleo STM32F746 and have a problem with in-circuit flash programming. The flash drivers used have been in various other STM32 M3, M4 and M7 parts without any issues (since about 2010) but with the F746 the effect that I see is that...

hpipon957 by Associate III
  • 3716 Views
  • 8 replies
  • 0 kudos

x-cube AWS OTA fails (Solved)

Hello geeks....I'm using x-cube aws sdk with P-L496G-CELLONE development board SDK version is 1.4.0 having aws version 3.0.1I can successful connect with the my MQTT aws server Now the problem is, when i try to do OTA then, out of 5 attempts, 4 attem...

0693W000003Bs3lQAC.png

Resolved! Hi all, Is it possible to communicate between a STM32F429VGT6 in USB Host mode with a FTDI FT230XS chip?

We have already a product based on STM32F429VGT6 which uses USB Host feature to read out data from plugged in USB-memory sticks. Our device have an USB A input so that normal USB-sticks can be inserted.This works well.Now there is an USB-stick which ...

HPiel.1 by Associate II
  • 5763 Views
  • 9 replies
  • 0 kudos

Resolved! HAL_SPI_Receive() ... Source Code

HIcommunityI am new to the STM32 world and am looking for the name of the library file in which the function HAL_SPI_Receive (..) is included as source code or the direct source code of this function.thanks for help

PKyyy.1 by Associate
  • 1828 Views
  • 3 replies
  • 0 kudos

How do I debug Ethernet on STM32F767?

I've got my own design STM32F767 boards and I've briefly had the Ethernet going but now it's stopped working and I don't know where to look. I'm using CubeMX to generate the application framework and the hardware is basically a clone of the Nucleo bo...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.