2023-03-06 2:40 AM
looking into this community i see that
- azureRTOS https://community.st.com/s/topic/0TO3W0000004ZG8WAM/azurertos is under STM32 MCUs https://community.st.com/s/topic/0TO0X000000BSqSWAW/stm32-mcus
- FreeRTOS_MPU https://community.st.com/s/topic/0TO0X0000005I9OWAU/freertosmpu is under STM32 MPUs https://community.st.com/s/topic/0TO0X0000003u2AWAQ/stm32-mpus
I don't really understand why FreeRTOS is not a sub topic for STM32 MCUs in the forum.
I looked into using FreeRTOS (in tickless mode) together with CubeMX and have the impression that the support for FreeRTOS in CubeMX is limited when it comes to regenerating code.
I didn't work with AzureRTOS (in tickless mode) before.
From what i did see in a STM32C0 workshop FreeRTOS is not really a topic but AzureRTOS is promoted.
My questions to STM and the community:
- Is / will FreeRTOS for STM32 MCUs really be supported by STM ?
- Are the problems named in https://nadler.com/embedded/newlibAndFreeRTOS.html worked on / solved by STM ?
- Will STM support AzureRTOS primarily ?
Can you tell about / compare practical experience with AzureRTOS / FreeRTOS (in tickless mode) for STM32 M0+ MCUs?
Solved! Go to Solution.
2023-03-06 7:46 AM
Hi @_richard ,
(sorry I don't have details on the newlib topic)
I hope it helps.
Kind Regards,
2023-03-06 7:46 AM
Hi @_richard ,
(sorry I don't have details on the newlib topic)
I hope it helps.
Kind Regards,
2023-03-09 1:52 AM
Thanks for your answer
in my case the native mode for FreeRTOS is needed (L0 hardware). as far as i see it now the xcube code generation can overwrite some necessary changes. see stm video concerning freertos.
the newlib question is interesting to me as this at the beginning of a project.
and i see no X-CUBE-AZRTOS-L0 package.
this would be interesting as maybe later a change to L4 may be needed. having built on FreeRTOS may be a disadvantage then, with freertos not getting primary support and open newlib question.
-> will X-CUBE-AZRTOS-L0 become avaliable soon (together with X-CUBE-AZRTOS-C0) ?
2023-03-09 2:20 AM
Hi @_richard
Both L0 and L4 don't need any X-CUBE-FREERTOS package, since they remain supported by the native mode on STM32CubeMX with native FreeRTOS.
So if your target is L0/L4 you don't need to change anything.
The changes I mentioned above are relative only to new series released after STM32U5 (ie. STM32U5, STM32H5, STM32C0, ...)
2023-03-09 2:40 AM
i understand that in my case the native mode for FreeRTOS is needed -> ther is still the code generation issue mentioned.
my newlib question and the question concerning X-CUBE-AZRTOS-L0 package are still open
best regards
richard
2023-03-09 4:18 AM
OK let's manage each point separately:
1. There is no X-CUBE-AZRTOS for L0 (and nothing is planned in the future). X-CUBE-AZRTOS is deployed only on following series: STM32H7, STM32F7, STM32F4, STM32L4, STM32L5, STM32G4, STM32G0, STM32WB, STM32WL.
No other series are concerned by X-CUBE-AZRTOS package.
As I explained before, of course, all new STM32 series (STM32U5, STM32H5, STM32C0, ...) get Azure RTOS middleware natively and do not also need X-CUBE-AZRTOS package.
2. NewLib : Could you please precise your issue exactly ? (for example is it using malloc inside USB stack ? or other ?)
2023-03-09 4:44 AM
1)
yes,
i see there is no X-CUBE-AZRTOS-L0 package ->
will X-CUBE-AZRTOS-L0 become available soon (together with X-CUBE-AZRTOS-C0) ?
2)
it is a new project. i can not answer now how the code will look.
my impression is that mr. nadler knows the topic and that his remarks in https://nadler.com/embedded/newlibAndFreeRTOS.html could become relevant. I thought that STM might have an answer on that.
2023-03-09 5:09 AM
1) I can confidently confirm that there is and there will be no X-CUBE-AZRTOS-L0 in the foreseen future.
2) I can't answer directly mr. Nadler. I respect his point of view, but there are points raised in that post that are not correct or not relevant or no more relevant today.
I suggest that you build your project and check by yourself and if you find any issues, we're here to help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.