2019-05-19 1:49 PM
I have started from blinky project and want to extend it for some PWM outputs on TIM2.
For this I need to make use of stm32f3xx_ll_tim.h.
I added into my main.c #include <stm32f3xx_ll_tim.h> without success
I added the file from 'Manage project Items' also without success!
Is the only way to add this driver over 'Manage Run-Time Environment'? The problem from this wizard I dont know which menu should I add in order to have this driver in my project!
Could anyone please help?
2019-05-22 5:35 AM
OK, thanks.
But even if I need them only in my main.c?
Could you please help for the other point?
So the problem is now after defining them from command line, then I can success compiling the project (build f7), but I fail to link it (Batch Build)!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.