2019-07-10 9:37 PM
Different sources give different and/or ambiguous information on ADC internal connections.
Take VREFINT on G474 for example.
Datasheet (DS12288 Rev 1) Section 3.18.2 Internal voltage reference (VREFINT) say
Reference manual (RM0440 Rev 1) Section 20.4.33 Monitoring the internal voltage reference say
FW1.0.0 stm32g4xx_hal_adc.h suggest
Similar confusion on internal temperature sensor. In this case, FW1.0.0 stm32g4xx_hal_adc.h is saying two different things in comments for channel identifiers.
It is unclear which connection(s) are actually connected for devices with ADC1 and ADC5.
2019-07-29 3:14 AM
Dear Yoichi,
I think you are refering to RM0440 "20.4.33 Monitoring the internal voltage reference". As you guessed it, ADC1_INP0 is not correct.
I raised a ticket for that.
Related to VREFINT, as you mentionned, it is available on ADCx_IN18, x = 1,3,4,5 input channels.
Related to Temperature Sensing, it is available on both, ADC1 Channel 16, and ADC5 channel 4, for devices with ADC1 and ADC5.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.