2018-09-05 1:15 AM
I'm using NUCLEO-446ZE Host to access USB Keyboard
My cubeMx version STM32Cube FW_F4 V1.21.0
I configured all clock and 48Mhz for USB via PLLSAIP
Main core run on 180Mhz
While connecting Keyboard I'm able to detect
While accessing
k_pinfo = USBH_HID_GetKeybdInfo(&hUsbHostFS);
at first the structure return ok and no data
but from seconds cycle the the k_pinfo is always NULL
while debugging I get to know that the fifio head and tail are 0
and
HID_HandleTypeDef *HID_Handle = (HID_HandleTypeDef *) phost->pActiveClass->pData;
HID_Handle->Length = 2 always
Kindly suggest any rectification
My main.c
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stm32f4xx_hal.h"
#include "usart.h"
#include "usb_host.h"
#include "gpio.h"
/* USER CODE BEGIN Includes */
#include "usbh_hid.h"
#include "usbh_hid_parser.h"
/* USER CODE END Includes */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void MX_USB_HOST_Process(void);
/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*/
/* USER CODE END PFP */
/* USER CODE BEGIN 0 */
extern ApplicationTypeDef Appli_state;
extern USBH_HandleTypeDef hUsbHostFS;
HID_KEYBD_Info_TypeDef * k_pinfo;
__IO char c;
__IO uint8_t once = 0;
/* USER CODE END 0 */
/**
* @brief The application entry point.
*
* @retval None
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART3_UART_Init();
MX_USB_HOST_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
MX_USB_HOST_Process();
/* USER CODE BEGIN 3 */
if(Appli_state == APPLICATION_READY){
HAL_GPIO_WritePin(GPIOB, LD3_Pin, GPIO_PIN_SET);
USBH_HID_GetPollInterval(&hUsbHostFS);
}
else{
HAL_GPIO_WritePin(GPIOB, LD3_Pin, GPIO_PIN_RESET);
}
if(Appli_state == APPLICATION_READY){
if(USBH_HID_GetDeviceType(&hUsbHostFS) == HID_KEYBOARD){
//HAL_GPIO_WritePin(GPIOB, LD2_Pin, GPIO_PIN_SET);
k_pinfo = USBH_HID_GetKeybdInfo(&hUsbHostFS);
if(k_pinfo != NULL)
{
c = USBH_HID_GetASCIICode(k_pinfo);
if(c != 0)
{
HAL_GPIO_WritePin(GPIOB, LD2_Pin, GPIO_PIN_SET);
HAL_Delay(10);
HAL_GPIO_WritePin(GPIOB, LD2_Pin, GPIO_PIN_RESET);
}
}
}
else{
HAL_GPIO_WritePin(GPIOB, LD3_Pin, GPIO_PIN_RESET);
}
}
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;
/**Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 180;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 7;
RCC_OscInitStruct.PLL.PLLR = 2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Activate the Over-Drive mode
*/
if (HAL_PWREx_EnableOverDrive() != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_CLK48;
PeriphClkInitStruct.PLLSAI.PLLSAIM = 4;
PeriphClkInitStruct.PLLSAI.PLLSAIN = 96;
PeriphClkInitStruct.PLLSAI.PLLSAIQ = 2;
PeriphClkInitStruct.PLLSAI.PLLSAIP = RCC_PLLSAIP_DIV4;
PeriphClkInitStruct.PLLSAIDivQ = 1;
PeriphClkInitStruct.Clk48ClockSelection = RCC_CLK48CLKSOURCE_PLLSAIP;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure the Systick interrupt time
*/
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
/**Configure the Systick
*/
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
/* USER CODE BEGIN 4 */
void USBH_HID_EventCallback(USBH_HandleTypeDef *phost){
HAL_GPIO_WritePin(GPIOB, LD2_Pin, GPIO_PIN_SET);
HAL_Delay(10);
HAL_GPIO_WritePin(GPIOB, LD2_Pin, GPIO_PIN_RESET);
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @param file: The file name as string.
* @param line: The line in file as a number.
* @retval None
*/
void _Error_Handler(char *file, int line)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
while(1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
2018-09-05 9:28 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.