2019-11-08 11:40 PM
switch (phost->gState)
{
case HOST_IDLE :
if (phost->device.is_connected)
{
USBH_UsrLog("USB Device Connected");
/* Wait for 200 ms after connection */
phost->gState = HOST_DEV_WAIT_FOR_ATTACHMENT;
USBH_Delay(200U);
USBH_LL_ResetPort(phost);
#if (USBH_USE_OS == 1U)
phost->os_msg = (uint32_t)USBH_PORT_EVENT;
#if (osCMSIS < 0x20000U)
(void)osMessagePut(phost->os_event, phost->os_msg, 0U);
#else
(void)osMessageQueuePut(phost->os_event, &phost->os_msg, 0U, NULL);
#endif
#endif
}
break;
case HOST_DEV_WAIT_FOR_ATTACHMENT: /* Wait for Port Enabled */
if (phost->device.PortEnabled == 1U)
{
USBH_UsrLog("USB Device Reset Completed");
phost->gState = HOST_DEV_ATTACHED;
}
break;
case HOST_DEV_ATTACHED :
if (phost->pUser != NULL)
{
phost->pUser(phost, HOST_USER_CONNECTION);
}
/* Wait for 100 ms after Reset */
USBH_Delay(100U);
phost->device.speed = USBH_LL_GetSpeed(phost);
phost->gState = HOST_ENUMERATION;
phost->Control.pipe_out = USBH_AllocPipe(phost, 0x00U);
phost->Control.pipe_in = USBH_AllocPipe(phost, 0x80U);
/* Open Control pipes */
USBH_OpenPipe(phost,
phost->Control.pipe_in,
0x80U,
phost->device.address,
phost->device.speed,
USBH_EP_CONTROL,
(uint16_t)phost->Control.pipe_size);
/* Open Control pipes */
USBH_OpenPipe(phost,
phost->Control.pipe_out,
0x00U,
phost->device.address,
phost->device.speed,
USBH_EP_CONTROL,
(uint16_t)phost->Control.pipe_size);
#if (USBH_USE_OS == 1U)
phost->os_msg = (uint32_t)USBH_PORT_EVENT;
#if (osCMSIS < 0x20000U)
(void)osMessagePut(phost->os_event, phost->os_msg, 0U);
#else
(void)osMessageQueuePut(phost->os_event, &phost->os_msg, 0U, NULL);
#endif
#endif
break;
case HOST_ENUMERATION:
/* Check for enumeration status */
if (USBH_HandleEnum(phost) == USBH_OK)
{
/* The function shall return USBH_OK when full enumeration is complete */
USBH_UsrLog("Enumeration done.");
phost->device.current_interface = 0U;
if (phost->device.DevDesc.bNumConfigurations == 1U)
{
USBH_UsrLog("This device has only 1 configuration.");
phost->gState = HOST_SET_CONFIGURATION;
}
else
{
phost->gState = HOST_INPUT;
}
}
break;
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.