2020-07-21 5:40 AM
If the Nucleo-H743ZI2 is newer, why Nucleo-H743ZI is the active version? I have a Nucleo-H743ZI2 board. So, where can I find schematic and support page for Nucleo-H743ZI2?
2020-07-21 6:47 AM
The ZI2 has the ST-LINK/V3 and the V-step STM32H743 capable of 480 MHz operation.
Handful of pins, including LEDs have changed. The .H files for the BSP look for a command line define.
2020-07-21 7:10 AM
NUCLEO-H743ZI (MB1137)
NUCLEO-H743ZI2 (MB1364)
#if defined (USE_NUCLEO_H745ZI_Q) || defined (USE_NUCLEO_H743ZI2) || defined (USE_NUCLEO_H7A3ZI_Q)
#define LED2_PIN GPIO_PIN_1
#define LED2_GPIO_PORT GPIOE
#define LED2_GPIO_CLK_ENABLE() __HAL_RCC_GPIOE_CLK_ENABLE()
#define LED2_GPIO_CLK_DISABLE() __HAL_RCC_GPIOE_CLK_DISABLE()
#else /* USE_NUCLEO_H743ZI */
#define LED2_PIN GPIO_PIN_7
#define LED2_GPIO_PORT GPIOB
#define LED2_GPIO_CLK_ENABLE() __HAL_RCC_GPIOB_CLK_ENABLE()
#define LED2_GPIO_CLK_DISABLE() __HAL_RCC_GPIOB_CLK_DISABLE()
#endif
/**
* @brief SD Control Interface pins (shield D4)
*/
#define ADAFRUIT_802_SD_CS_PIN GPIO_PIN_14
#if defined (USE_NUCLEO_H745ZI_Q) || defined (USE_NUCLEO_H743ZI2) || defined (USE_NUCLEO_H7A3ZI)
#define ADAFRUIT_802_SD_CS_GPIO_PORT GPIOE
#define ADAFRUIT_802_SD_CS_GPIO_CLK_ENABLE() __HAL_RCC_GPIOE_CLK_ENABLE()
#define ADAFRUIT_802_SD_CS_GPIO_CLK_DISABLE() __HAL_RCC_GPIOE_CLK_DISABLE()
#else /* USE_NUCLEO_H743ZI */
#define ADAFRUIT_802_SD_CS_GPIO_PORT GPIOF
#define ADAFRUIT_802_SD_CS_GPIO_CLK_ENABLE() __HAL_RCC_GPIOF_CLK_ENABLE()
#define ADAFRUIT_802_SD_CS_GPIO_CLK_DISABLE() __HAL_RCC_GPIOF_CLK_DISABLE()
#endif
/**
* @brief LCD Control Interface pins (shield D10)
*/
#define ADAFRUIT_802_LCD_CS_PIN GPIO_PIN_14
#define ADAFRUIT_802_LCD_CS_GPIO_PORT GPIOD
#define ADAFRUIT_802_LCD_CS_GPIO_CLK_ENABLE() __HAL_RCC_GPIOD_CLK_ENABLE()
#define ADAFRUIT_802_LCD_CS_GPIO_CLK_DISABLE() __HAL_RCC_GPIOD_CLK_DISABLE()
/**
* @brief LCD Data/Command Interface pins (shield D8)
*/
#if defined (USE_NUCLEO_H743ZI2) || defined (USE_NUCLEO_H7A3ZI)
#define ADAFRUIT_802_LCD_DC_PIN GPIO_PIN_3
#define ADAFRUIT_802_LCD_DC_GPIO_PORT GPIOF
#define ADAFRUIT_802_LCD_DC_GPIO_CLK_ENABLE() __HAL_RCC_GPIOF_CLK_ENABLE()
#define ADAFRUIT_802_LCD_DC_GPIO_CLK_DISABLE() __HAL_RCC_GPIOF_CLK_DISABLE()
#elif defined (USE_NUCLEO_H745ZI_Q)
#define ADAFRUIT_802_LCD_DC_PIN GPIO_PIN_9
#define ADAFRUIT_802_LCD_DC_GPIO_PORT GPIOG
#define ADAFRUIT_802_LCD_DC_GPIO_CLK_ENABLE() __HAL_RCC_GPIOG_CLK_ENABLE()
#define ADAFRUIT_802_LCD_DC_GPIO_CLK_DISABLE() __HAL_RCC_GPIOG_CLK_DISABLE()
#else /* USE_NUCLEO_H743ZI */
#define ADAFRUIT_802_LCD_DC_PIN GPIO_PIN_12
#define ADAFRUIT_802_LCD_DC_GPIO_PORT GPIOF
#define ADAFRUIT_802_LCD_DC_GPIO_CLK_ENABLE() __HAL_RCC_GPIOF_CLK_ENABLE()
#define ADAFRUIT_802_LCD_DC_GPIO_CLK_DISABLE() __HAL_RCC_GPIOF_CLK_DISABLE()
#endif
/**
* @brief ADC Interface pins
* used to detect motion of Joystick available on Adafruit 1.8" TFT shield
*/
#if defined (USE_NUCLEO_H745ZI_Q) || defined (USE_NUCLEO_H743ZI2) || defined (USE_NUCLEO_H7A3ZI)
#define ADAFRUIT_802_ADCx ADC1
#define ADAFRUIT_802_ADCx_CLK_ENABLE() __HAL_RCC_ADC12_CLK_ENABLE()
#define ADAFRUIT_802_ADCx_CLK_DISABLE() __HAL_RCC_ADC12_CLK_DISABLE()
#define ADAFRUIT_802_ADCx_CHANNEL ADC_CHANNEL_5
#define ADAFRUIT_802_ADCx_GPIO_PORT GPIOB
#define ADAFRUIT_802_ADCx_GPIO_PIN GPIO_PIN_1
#define ADAFRUIT_802_ADCx_GPIO_CLK_ENABLE() __HAL_RCC_GPIOB_CLK_ENABLE()
#define ADAFRUIT_802_ADCx_GPIO_CLK_DISABLE() __HAL_RCC_GPIOB_CLK_DISABLE()
#else /* USE_NUCLEO_H743ZI */
#define ADAFRUIT_802_ADCx ADC3
#define ADAFRUIT_802_ADCx_CLK_ENABLE() __HAL_RCC_ADC3_CLK_ENABLE()
#define ADAFRUIT_802_ADCx_CLK_DISABLE() __HAL_RCC_ADC3_CLK_DISABLE()
#define ADAFRUIT_802_ADCx_CHANNEL ADC_CHANNEL_5
#define ADAFRUIT_802_ADCx_GPIO_PORT GPIOF
#define ADAFRUIT_802_ADCx_GPIO_PIN GPIO_PIN_3
#define ADAFRUIT_802_ADCx_GPIO_CLK_ENABLE() __HAL_RCC_GPIOF_CLK_ENABLE()
#define ADAFRUIT_802_ADCx_GPIO_CLK_DISABLE() __HAL_RCC_GPIOF_CLK_DISABLE()
#endif
2020-07-21 7:12 AM
Hi @Community member ,
Board reference for Nucleo-H743ZI2 is MB1364.
Helpful documents on this regard are:
You can have a look to this discussion as well: https://community.st.com/s/question/0D53W00000BuOJ6SAN.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-07-21 9:26 AM
Ohh, really fast! :) Thank you Amel and Clive!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.