2023-12-03 3:43 AM
Scenario:
Windows 11 connected to Nucleo-L476RG.
Fresh install of STMCubeIDE
Version: 1.14.0
Build: 19471_20231121_1200 (UTC)
OS: Windows 11, v.10.0, x86_64 / win32
Ran STLinkUpgrade 3.13.4
Result: Update to Firmware: V2J43M28 STM Debug+Mass storage+VCP Upgrade successful.
File > New STM Project
Selected board L476RG
Project name testtest
Initialised all peripherals with default.
Configurator opened main.c
Project > Build Project
11:30:19 Build Finished. 0 errors, 0 warnings. (took 3s.143ms)
Error in final launch sequence:
Failed to start GDB server
Failed to start GDB server
Error in initializing ST-LINK device.
Reason: (0) Unknown. Please check power and cabling to target.
Failed to bind to port 61235, error code -1: No error
Failure starting SWV server on TCP port: 61235
Failed to bind to port 61234, error code -1: No error
Failure starting GDB server: TCP port 61234 not available.
Shutting down...
Exit.
My question:
The cable is a known good one, and the STLink upgrade was successful, so it seems to me that there is nothing wrong with
Solved! Go to Solution.
2023-12-03 4:36 AM - edited 2023-12-03 7:36 AM
Solved! And I think I know what the problem might be.
From the Windows "Add & Remove Programs" menu I removed anything with ST in the name and did another fresh installation. This time I got the message "Do you want to allow public and private networks to access this app? Windows Firewall has blocked some features of st-link_gdbserver.exe on all public and private networks".
I have not seen this message before.
I clicked "Allow" and the installation continued, and now it works.
Another Sunday wasted - ho-hum
ADDED LATER: on reflection, in the process of uninstalling I uninstalled 2 versions of STMCubeIDE as well as one STLink file. It's possible the problem was related to that, as per the links above. Either way, a complete uninstall / reinstall fixed it
2023-12-03 4:09 AM
By the way, I know both my Nucleo board and the cable are good as they work on my Linux machine
2023-12-03 4:17 AM
2023-12-03 4:36 AM - edited 2023-12-03 7:36 AM
Solved! And I think I know what the problem might be.
From the Windows "Add & Remove Programs" menu I removed anything with ST in the name and did another fresh installation. This time I got the message "Do you want to allow public and private networks to access this app? Windows Firewall has blocked some features of st-link_gdbserver.exe on all public and private networks".
I have not seen this message before.
I clicked "Allow" and the installation continued, and now it works.
Another Sunday wasted - ho-hum
ADDED LATER: on reflection, in the process of uninstalling I uninstalled 2 versions of STMCubeIDE as well as one STLink file. It's possible the problem was related to that, as per the links above. Either way, a complete uninstall / reinstall fixed it
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.