2018-02-05 8:00 AM
Hi,
i swapped my first STM32F407G-DISC1 discovery board for a new one and now the ST-Link onboard doesnt show up as a virtual com port in Windows 10 anymore.
I flashed the St-Link with the new firmware, it runs V2.J30.S0 STM32 Debugger now.
I also installed the current Windows driver from
.Now i read the DISCOVERY boards dont all have the virtual com, but in
http://www.st.com/en/evaluation-tools/stm32f4discovery.html
it says that my order code should have it (on my PCB is a silk print next to the USB connector that says 'STM32F407G-DISC1).Can it be that the silkscreen board code doesnt correspond to the 'order code' which is mentioned on the above website?
Please help since i really need the virtual COM port.
Patrick
#st-link-v2-1 #stm32f746-discovery #stm32f42018-02-05 8:06 AM
Run St-link utility to see firmware version. v2-1 is required (in this case v2-B
2018-02-05 8:13 AM
The latest (DISC1) version shall have the st-link based on STM32F103CBT6 - the old - STM32F103C8T6. Flash size matters - bigger flash is needed for the ST-link/v2-B where the VCOM is implemented
2018-02-05 8:26 AM
Are they different board revisions?
Pretty sure the MB997D instantiates the VCP, but it's not physically wired up to anything.
2018-02-05 9:37 AM
Are you sure that MB997D applies to STMF429-DISC1?
Isn't it STM32F407G-DISC1 which has the MB997D?
2018-02-05 9:40 AM
Sorry - I have noticed that the boards is really F407
2018-02-12 2:19 AM
Hi,
i have two boards, one of them doesnt instantiate the VCOM port, it has:
10:14:12 : ST-LINK SN : 066FFF535748775187133407
10:14:12 : ST-LINK Firmware version : V2J30S0
and the other board does instantiate it and has:
10:17:19 : ST-LINK SN : 066BFF3731324B4D43205239
10:17:19 : ST-LINK Firmware version : V2J25M14Both boards are labeled MB997D / STM32F407G-DISC1 on the silkscreen and St-Link shows RevisionID: Rev 2.0 for both of them.
Can i upgrade the firmware of the non-working one to the firmware
V2J25M14 or does it not fit the flash size?
2018-02-12 2:28 AM
The standard way is to run ST-LINK Utility and see after connecting to the target if the red message appears in the log - it will be stated if the upgrade is possible.
Just run the utility to see the checking results. Then you can upgrade the firmware from the same utility - 'ST-LINK->Firmware Update' (sometimes you need to re-plug the USB cable when the tools complains about the connectivity).
If this does not help (I mean the ST-LINK Utility) more investigation will be required.
2018-02-12 2:35 AM
When i connect the board, ST-Link gives me this output:
10:32:58 : ST-LINK SN : 066FFF535748775187133407
10:32:58 : ST-LINK Firmware version : V2J30S010:32:58 : Connected via SWD.10:32:58 : SWD Frequency = 4,0 MHz.10:32:58 : Connection mode : HotPlug.10:32:58 : Debug in Low Power mode enabled.10:32:58 : Device ID:0x413 10:32:58 : Device flash Size : 1MBytes10:32:58 : Device family :STM32F405xx/F407xx/F415xx/F417xxWhen i try to update the firmware, it says it can upgrade from 'V2.J30.S0 STM32 Debugger' to 'V2.J27.S0'
2018-02-12 2:36 AM
It's somewhat weird - these firmwares come from two different lines.
Please check what the MCU is soldered for the ST-LINK: STM32F103C8T6 OR STM32F103CBT6?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.