2022-08-04 5:22 AM
Hello,
i am trying to program a STM32G031. unfortunately it does not work with cubeIDE i want to use for. please see the following message from the console:
STMicroelectronics ST-LINK GDB server. Version 7.0.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.11.0-RC1
-------------------------------------------------------------------
Log output file: C:\Users\PETE\AppData\Local\Temp\STM32CubeProgrammer_a07592.log
ST-LINK SN : 55FF6D067880565348432067
ST-LINK FW : V2J40S7
Board : --
Voltage : 3.21V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x466
Revision ID : Rev 1.1
Error: Database: There's no active configuration for this device. All the 6 configurations are disabled!
Error: Database: There's no active configuration for this device. All the 6 configurations are disabled!
Device name : STM32G03x/STM32G04x
Flash size : 63 KBytes (default)
Device type : MCU
Device CPU : Cortex-M0+
BL Version : --
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a07592.srec
File : ST-LINK_GDB_server_a07592.srec
Size : 11.37 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing external memory sectors [0 5]
File segment @0x08000000 is not 255-bytes aligned. It will be aligned to @0x07FFFFF8
Download in Progress:
Error: failed to download Segment[0]
Error: failed to download the File
Shutting down...
Exit.With the Keil software the programming works with the same ST-Link V2 but without further problems. So the problem is a incorrect setting in the debug configurations?
2023-01-30 2:59 AM
Hi @Samweis,
Did you solve this?
Looks like a CubeProgrammer issue.
2023-04-25 7:50 PM
I'm getting the same error. It was happening with STM32CubeProgrammer v2.13 both standalone and in the IDE, so I downgraded to v2.10. Now standalone works fine but IDE still gives the same error, even in v2.10, which I find a little stange.
Something I noticed is that the standalone programmer writes to 0x08000000 while the IDE one aligns it to 0x07FFFFF8 for some reason. Do you think that could be the issue?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.