2022-03-16 9:41 AM
Since the most current and the previous version of STM32CubeIDE (or maybe related to a windows 10 update) I have to start the debug session 2 times. The first time the error below is produced. If I however start it a second time, everything works. The error occurs after a few seconds. Can I increase a timeout somewhere? Does anybody else have the same problem?
Error in final launch sequence:
Failed to execute MI command:
target remote localhost:60000
Error message from debugger back end:
localhost:60000: Connection timed out.
Failed to execute MI command:
target remote localhost:60000
Error message from debugger back end:
localhost:60000: Connection timed out.
localhost:60000: Connection timed out.
2022-03-16 11:08 AM
> Does anybody else have the same problem?
Don't have much to add other than it works okay here using STM32F429, STLINK-V3MINI, CubeIDE, GDB, Win10.
Might try lowering the frequency under debug configuration options.
2022-03-16 1:26 PM
It happens if I activate "use RTOS proxy", which is needed to show code positions in all RTOS threads if the program is paused. It occurs with both, OpenOCD and GDB server.
2023-01-25 7:43 AM
Hi @awiernie ,
Did you ever solve this one?
There was an issue with Eclipse/CDT in previous versions where the shutdown of debug sessions on Windows was not always clean. We up-stream a bug fix to Eclipse/CDT on this to fix this issue. I think that the bug fix is part of CubeIDE 1.10.x and later....
2023-01-28 12:52 PM
The issue is still present on CubeIDE 1.11.0 - Most of the time I have two start debug session 2times, because the first will time out most times.
2024-03-15 2:38 AM
The problem occured only in combination with rtos thread debugging. I can avoid this problem if I disable automake in the debugger settings.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.