2017-11-28 2:03 AM
I have a STM32091C-EVAL board, and I'm trying to get console output on the STLink-2.1 debug console interface throught USART5, but I have no output by the STLink.
- I have updated the STLink firmware to the latest 2.29.18, no effect
- I took the USART5 signals from the
CN6
header, I have correct console output- I soldered an header on the CN17 header, right before the stlink, after the U17, nothing, output line is allways at 0
I suspect the level shifter to be faulty, because the voltages on the level shifter pins are OK.
Anybody got the same issue ? is it only on my board ?
#stlink #stm32f0 #stm32091c-eval2017-11-30 3:11 PM
So you see the correct Tx waveform on pin 2 of U17, and a steady level on pin 7 of U17? And there are correct power supply voltages on pins 1 and 8 of U17?
JW
2017-12-06 4:12 AM
Hi
Waclawek.Jan
,Yes, power supply is correct on pins 1 and 8.
Is there a way to contact ST to do a return ?
Neil
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.