2025-07-31 1:38 PM
STLINK V3 stopped working after upgrade. Red light is flashing. Device manager - Unknown USB Device. NUCLO and DISCOVERY with ST-Link2 are still working! Installing dpinst_amd64.exe not help.
Solved! Go to Solution.
2025-07-31 2:26 PM
Thanks, I have already removed USB hub. Yes, I replace the cable and it is working now.
Thank you very much. How can upgrade brake the cable?!
2025-07-31 2:12 PM
If red light is flashing, it indicates enumeration is failing. Try a different cable or adding/removing a USB hub from the chain.
2025-07-31 2:26 PM
Thanks, I have already removed USB hub. Yes, I replace the cable and it is working now.
Thank you very much. How can upgrade brake the cable?!
2025-07-31 3:02 PM
Operates at a faster rate, say 480 Mbps vs 12 Mbps, and then the cable quality/performance becomes much more of an issue..
2025-07-31 3:42 PM - edited 2025-07-31 3:43 PM
The upgrade cannot break the cable.
Just because something "works" doesn't mean there are no issues.
2025-07-31 8:40 PM
I took another similar cable an it start working right away. Let see how it will go.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.