2021-04-28 1:50 PM
It fails at 24MHz, but mostly works at 8MHz. Is there a spec on it somewhere?
Solved! Go to Solution.
2021-04-28 2:02 PM
Chart says SWD 12 MHz
"Table 19. Achievable maximal performance with STLINK-V3SET on different channels"
2021-04-28 2:02 PM
Chart says SWD 12 MHz
"Table 19. Achievable maximal performance with STLINK-V3SET on different channels"
2021-04-29 12:43 AM
OK - 8MHz. Many thanks.
Curiously that table states 16MHz for the SWV, while Cube IDE supports a max speed of 2MHz. Getting this to go faster would be useful because it affects the execution speed of SWV ITM debug output; you want maximum speed on that.
2021-05-11 9:41 AM
I did some tests, on straight code loading, no debugging etc, and the ISOL board bombs out around 18MHz. This is probably cabling dependent.
Note that there is a weird problem with the connector usage
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.