2013-02-04 10:05 PM
Hi All,
I am using Keil uVision 4 with the ST-Link in the STM32L Discovery board. I can load a 150K binary on my windows machine in less than a minute but on my virtual machine it takes close to 4 minutes! The virtual machine is running on a macbook pro with beefy specs [ 2GHz Quad i7 with 12GB RAM , 4Gb for the VM and a SSD hard drive ] . I know the specs dont matter as much for the transfer speed but I cannot figure out why the performance would be so different. I am flashing using SWD [ not JTAG ] not sure if that makes a diff either. Any help here is appreciated! Thanks #st-link #stm32-discovery2013-02-05 8:14 AM
It could be a protocol issue, or USB visualization issue. Are you using Virtual Box, or can you try another VM.
I've used Segger J-Link's under Virtual Box, and I can't say I perceived any chronic drag on it. But an Apples and Oranges comparison there. Six cored Phenom II X6 1035T with 16GB It could be ST-Link specific, suggest you try a U-Link or J-Link before you give up on the virtualization.2013-02-05 1:51 PM
i am using parallels 8. Not sure if this has to do with the beefiness of the machine . Also the same ST-Link works great on a native windows desktop.
I did try J-Link which was definitely better but still wasn't up to speed with what I saw on the desktop. I realized I can get a shitty windows machine for less than what the J-Link costs and get the same performance as the ST-Link !2013-02-05 3:48 PM
Not sure if this has to do with the beefiness of the machine.
Pretty sure it doesn't.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.