2022-03-04 1:00 PM
2022-03-07 5:03 PM
Updating this post as I have since found a solution, attaching wires to the contacts of the solder bridge allowed me to make a jumper circuit. When programming the device the pins must be shorted, these can then be separated when running.
2022-03-04 1:03 PM
Edit: oh, you're still using the onboard ST-Link.
Should work, what error message or issue are you running into? You will need to ensure SWDIO/SWCLK are not reprogrammed, the chip doesn't enter low power states, otherwise you will need to boot up into the bootloader to connect.
2022-03-04 1:14 PM
This is what I get in MBED studio, interestingly, it seems to work despite the error maybe 1 out of 30 times?
2022-03-04 1:15 PM
Replied to myself accidentally, see my comment below, thanks.
2022-03-04 1:17 PM
Sounds like a software issue rather than a hardware one. Perhaps the debugger is assuming NRST is connected. If STM32CubeProgrammer can connect, issue isn't with the hardware connection.
2022-03-04 1:20 PM
No success with Cube:
2022-03-07 5:03 PM
Updating this post as I have since found a solution, attaching wires to the contacts of the solder bridge allowed me to make a jumper circuit. When programming the device the pins must be shorted, these can then be separated when running.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.