cancel
Showing results for 
Search instead for 
Did you mean: 

"UM2407 User manual", table 20, "CN9 ZIO Connector pinout" pin name of pin 15 wrong

CKok.1
Associate

Table 20, "CN9 ZIO Connector pinout" on page 40 of "UM2407 User manual Rev 2 - STM32H Nucleo-144 boards (MB1364)" lists the wrong pin name for pin CN9-15. It is listing PE0 while it should be listing PE9.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hi @CKok.1​ ,

I reported the issue: Table 20 should be wrong as the PE9 is used as COMP2_INP (Pin 15) on the ST Zio connector CN9.

Internal ticket number: 131478 (This is an internal tracking number and is not accessible or usable by customers).

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
KDJEM.1
ST Employee

Hi @CKok.1​ ,

I reported the issue: Table 20 should be wrong as the PE9 is used as COMP2_INP (Pin 15) on the ST Zio connector CN9.

Internal ticket number: 131478 (This is an internal tracking number and is not accessible or usable by customers).

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

KDJEM.1
ST Employee

Hello @CKok.1 ;

 

The issue is fixed in UM2407 Rev5.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.