2020-04-15 11:13 PM
STM32 Cube IDE throws failure message "Failed to list debug probes" when scanning for ST-LINK S/N under Debug Configurations/Debugger/GDB Server Command Line Options/Interface.
Problem has presented itself in last hour. It was working with a Nucleo-F042K6 and now not working with either the Nucelo-F042K6 and a Nucleo-F746ZG.
Trying to debug code that incorporates FreeRTOS Middleware utilising CMSIS_V2 hence the move to the significantly more powerful Nucleo-F746ZG as I realised RTOS is not compatible with the Nucelo-F042K6.
Ran ST-LINK Upgrade successfully on both boards.
Code compiled and downloaded from online mbed compiler works so I expect it is not an issue with the board.
Any assitance would be greatly appreciated.
2020-04-19 5:48 PM
Problem found to be Avast Antivirus, uninstalling STM32 Cube IDE and Avast and then reinstalling STM32 Cube IDE fixed the problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.