2023-09-12 5:52 AM
I would like to ask your team some of questions regarding the STM32 module kit which comes with BLE- 5.3 or BLE5.4, I want to make a device which works on BLE-5.3 or 5.4. I want to establish an AudioLE call by using your microcontrollers, Can I use AudioLE with any STM controller, If yes then how can I and if not then shall I do to make it work?
Will it work on full-duplex or half-duplex communication?
Can a 2 ways communication be possible using a single STM or will I need 2 STM to have a communication? Or can I use multiple channels with a single STM for communication?
Please answer these questions I have as soon as possible.
Thanks
Solved! Go to Solution.
2023-09-12 6:43 AM
Hello @yash_garg
I'm going to briefly answer your questions and then I will give some ressources that will help you:
First, you can create an Audio application using the STM32WB that integer a full-duplex bleutooth low energy communication between 2 STM32WB or an STM32WB and a mobile phone .
For more details, her is a demonstration of an application that may help you. Also, this video shows how audio interface in the WB works. And finally you can find her a function pack for STM32WB full-duplex audio streaming. You can use the joined to the pack exemples to discover more about. For more information, you can try to watch this video ( I think it use the Korean language but you can understand without the voice of) to now how it really works.
Best regards.
II
2023-09-12 6:43 AM
Hello @yash_garg
I'm going to briefly answer your questions and then I will give some ressources that will help you:
First, you can create an Audio application using the STM32WB that integer a full-duplex bleutooth low energy communication between 2 STM32WB or an STM32WB and a mobile phone .
For more details, her is a demonstration of an application that may help you. Also, this video shows how audio interface in the WB works. And finally you can find her a function pack for STM32WB full-duplex audio streaming. You can use the joined to the pack exemples to discover more about. For more information, you can try to watch this video ( I think it use the Korean language but you can understand without the voice of) to now how it really works.
Best regards.
II
2023-09-14 2:03 AM
can i use Audio Low Energy in STM32WB or not and if yes then will i need 2 MCU for making a device or one will be enough?
2023-09-14 2:07 AM
Hello again @yash_garg
Yes, you can use audio in stm32wb. You need just one stm32wb to do sol.
Best regards.
II
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.