cancel
Showing results for 
Search instead for 
Did you mean: 

Noise Injection via ST-Link Causing MCU Disturbance on STM32H743ZI

PrashantBhatta
Associate II

we are facing after migrating our design from STM32F405ZGT7 to STM32H743ZI.

We have an automotive application where a horn load creates significant EMI transients. With our previous design using STM32F405ZGT7, the system was stable and did not experience any MCU freezing or malfunction during horn activation.

However, after migrating to STM32H743ZI — while keeping the PCB layout, grounding strategy, power architecture, filtering components, and external circuitry identical — we began experiencing intermittent MCU freezing during horn actuation.

After extensive debugging and hardware validation, we observed the following:

The issue only occurs when ST-Link is connected.
When ST-Link is disconnected, the system behaves significantly more reliably.
The noise appears to be injected through the ST-Link interface path.
The horn generates high transient noise despite having local snubbers and filtering.
We have already implemented:
RC snubber across the horn load
EMI input filtering near MCU supply
Proper decoupling near all VDD pins
Ground plane continuity and star grounding where applicable

This behavior was not observed with STM32F405ZG under identical conditions.

We would like clarification on the following points:

Are there any known differences in debug interface robustness between STM32F405ZGT7 and STM32H743ZI?
Is the STM32H7 debug interface more sensitive to ground bounce or transient noise?
Are there recommended protection or isolation methods for ST-Link in high EMI automotive environments?
Is there any application note addressing EMI robustness of SWD/JTAG on STM32H7 series?

We suspect that higher core frequency, different internal architecture, or debug interface implementation in STM32H743ZI may be contributing to this sensitivity.

12 REPLIES 12

As suggested, I am sharing the power supply architecture and the STM32H743 circuit section for review.

I would like to clarify that the issue is not related to the ST-Link USB connection to the laptop.

The problem occurs even when the ST-Link USB is completely disconnected from the laptop (i.e., no USB cable connected).

What I have observed is:

  • The issue persists regardless of whether ST-Link is connected to a PC.

  • The MCU fails to recover with NRST and only recovers after a full power cycle.

  • The issue completely disappears if no external wires are taken out from the MCU board for SWDIO signals.

In other words, as soon as SWDIO lines are routed externally via wires (off-board connection), the problem becomes reproducible. If the SWDIO lines remain only on the PCB (no external wiring), the system operates normally.

So now clarified :

1. H743 running fine , no problems at all.

2. st-link debug also working ok.

3. Problem arises, if anything connected to debug-header on H743 board .

 

-> So you have 

a: bad ground connection H743-GND ---> st-link-GND

b: big spike coupling in/to the debug lines (even confusing the core )

 

-> improve H743-GND ---> st-link-GND connection, check for low impedance (!), short connection if possible.

or use screened wire for swd+swc , screen = GND on both sides .

If you feel a post has answered your question, please click "Accept as Solution".
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.