2017-04-03 9:14 AM
Hello,
When i connect my STM 32F401RE to the STM32 ST-Link Utility and then try to update the firmware, it says that Version V2.J27.M15 is the latest.
When i do the same with ST-Link Upgrade (stswlink007 from st.com), it says that Version V2.J28.M18 is the latest.
Which Firmware should i install now?
Best Regards
Armin
#st-link #st-link-utility #st-link-update2017-04-03 9:26 AM
Hi,
I recommend you to upgrade the ST-Link firmware version to V2-1 through this
Hope this help you.
Imen
2017-04-04 12:59 PM
>>
Which Firmware should i install now?
Does it matter? Do you have some issue that it might remediate? If it works, just leave it alone.
If you have a problem it makes sense to upgrade before complaining so that past issues aren't continually relitigated, but if things are working there is no need in most cases.
2017-04-04 1:55 PM
Thank yout both for your Quick Answers.
To the Thing with
/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fst_com%2Fen%2Fproducts%2Fembedded-software%2Fdevelopment-tool-software%2Fstsw-linkhtml
: I´ve already installed this and updated it with STSW-LINK007, or is there something about both Software´s i didn´t get?Yes I have a Issue with my board and i´m currently unsure about wether it´s a software or a hardware issue (my X-Nucleo-53L0A1 shield won´t work most times, just sometimes.....I know it sounds awkward but when i try figuring out whats the problem it feels like someone just rolling the dices about wether my shield will work or not, but i think i´m goint to open a new thread about that Problem tomorrow).
Thank you very much
2017-04-04 5:27 PM
They are on different release schedules and software released in the past will not have the most up-to-date firmware.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.