2022-02-07 5:55 AM
2022-02-10 4:26 AM
Ok, so the problem was that SCB->VTOR was not correctly set (even before HAL_Init() it still pointed to the beginning of FLASH - 0x0800...)
After HAL_Init() I've set
SCB->VTOR = (uint32_t)(0x24040000);
and SysTick interrupt works fine now.
Edit:
Ok, so a better implementation imo is to have in *FLASH.ld:
_eflash = ORIGIN(FLASH);
And in *.c something like:
extern uint32_t _eflash;
SCB->VTOR = (uint32_t)(_eflash);
2022-02-07 6:04 AM
I have a H743ZI2 nucleo board.
I've tried placing the FLASH section in RAM:
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
split in smth like:
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 256K
FLASH (xrw) : ORIGIN = 0x2A000000, LENGTH = 256K
or splitting RAM and placing sections which were previously in FLASH as:
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >SOME_NEW_RAM_REGION
either way it doesn't work (both ST-LINK GDB sv and OpenOCD).
Now, I know there is a previous q, essentially the same, but can someone please provide a detailed and steps to achieve this?
Thank you.
2022-02-07 6:07 AM
Error for OpenOCD:
Error: Failed to write memory at 0x2a000200
Error: Failed to write memory at 0x2a001898
2022-02-07 9:20 AM
You need better calculator 0x24000000 + 256k = 0x24040000
2022-02-08 4:56 AM
Ok, so in FLASH.ld:
MEMORY
{
/*FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 2048K*/
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 256K
FLASH (xrw) : ORIGIN = 0x24040000, LENGTH = 256K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
}
and RAM.ld:
MEMORY
{
RAM_EXEC (xrw) : ORIGIN = 0x24000000, LENGTH = 256K
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
}
I've tried setting breakpoints to void FLASH_IRQHandler(void), and further in other function pointers, execution does not break,
but flags are set in IRQ Handler, because execution is dependent on those flags and it behaves as expected.
Execution does not terminate cleanly, last stack state is:
Thread #1 [main] 1 [core: 0] (Suspended : Signal : SIGTRAP:Trace/breakpoint trap)
0x8000b32
<signal handler called>() at 0xfffffff9
0x0
flash_runnable() at TestFlash.c:127 0x240406aa
0x8000b32, is an address in flash region of uc.
Did I miss something, like relocating some mem regions, maybe vtor or?
2022-02-08 12:00 PM
2022-02-09 5:07 AM
I've read that post, at least for me, instructions are vague.
However, this is output from readelf cmd, suggested to be used in that post:
readelf -S Bootloader.elf
There are 23 section headers, starting at offset 0x1d9744:
Section Headers:
[Nr] Name Type Addr Off Size ES Flg Lk Inf Al
[ 0] NULL 00000000 000000 000000 00 0 0 0
[ 1] .isr_vector PROGBITS 24040000 010000 000298 00 A 0 0 1
[ 2] .text PROGBITS 24040298 010298 0050c0 00 AX 0 0 4
[ 3] .rodata PROGBITS 24045358 015358 000038 00 A 0 0 4
[ 4] .ARM ARM_EXIDX 24045390 015390 000008 00 AL 2 0 4
[ 5] .init_array INIT_ARRAY 24045398 015398 000004 04 WA 0 0 4
[ 6] .fini_array FINI_ARRAY 2404539c 01539c 000004 04 WA 0 0 4
[ 7] .data PROGBITS 24000000 020000 000014 00 WA 0 0 4
[ 8] .bss NOBITS 24000014 020014 000118 00 WA 0 0 4
[ 9] ._user_heap_stack NOBITS 2400012c 02012c 000604 00 WA 0 0 1
[10] .ARM.attributes ARM_ATTRIBUTES 00000000 020014 00002e 00 0 0 1
[11] .debug_info PROGBITS 00000000 020042 017bac 00 0 0 1
[12] .debug_abbrev PROGBITS 00000000 037bee 002b3e 00 0 0 1
[13] .debug_aranges PROGBITS 00000000 03a730 000ba8 00 0 0 8
[14] .debug_ranges PROGBITS 00000000 03b2d8 000ae0 00 0 0 8
[15] .debug_macro PROGBITS 00000000 03bdb8 035502 00 0 0 1
[16] .debug_line PROGBITS 00000000 0712ba 00e0e9 00 0 0 1
[17] .debug_str PROGBITS 00000000 07f3a3 153d00 01 MS 0 0 1
[18] .comment PROGBITS 00000000 1d30a3 000053 01 MS 0 0 1
[19] .debug_frame PROGBITS 00000000 1d30f8 002f1c 00 0 0 4
[20] .symtab SYMTAB 00000000 1d6014 002070 10 21 291 4
[21] .strtab STRTAB 00000000 1d8084 0015cd 00 0 0 1
[22] .shstrtab STRTAB 00000000 1d9651 0000f0 00 0 0 1
2022-02-10 4:26 AM
Ok, so the problem was that SCB->VTOR was not correctly set (even before HAL_Init() it still pointed to the beginning of FLASH - 0x0800...)
After HAL_Init() I've set
SCB->VTOR = (uint32_t)(0x24040000);
and SysTick interrupt works fine now.
Edit:
Ok, so a better implementation imo is to have in *FLASH.ld:
_eflash = ORIGIN(FLASH);
And in *.c something like:
extern uint32_t _eflash;
SCB->VTOR = (uint32_t)(_eflash);
2022-02-10 6:00 AM
Maybe when you read better system c file you see here lines
/*!< Uncomment the following line if you need to relocate your vector Table in
Internal SRAM. */
/* #define VECT_TAB_SRAM */
#define VECT_TAB_OFFSET 0x00 /*!< Vector Table base offset field.
This value must be a multiple of 0x200. */And entered valid values setup all in build for you...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.