2024-11-12 1:39 PM
Hello I am trying to currently flash and install a firmware file that is stored in a SD card in a STM32F746- Discovery board onto the board. I am new at working in this type the project the board its working as a mass storage device using the SD card as the storage and I want to be able to install any firmware files that is stored in the SD card tough an exe app I develop to be able and install it. I heard that using jumper it can be done, does anyone have any idea of how to do it or if anyone know any other way around.
Solved! Go to Solution.
2024-11-12 2:25 PM
You have to actually write the code to make the magic happen. The ROM based System Loader doesn't provide for this mode of operation. It provides for Serial connectivity, and for USB-DFU mode
See Application Note AN2606
Perhaps look at
STM32Cube_FW_F7_V1.17.1\Projects\STM32746G-Discovery\Applications\USB_Device\DFU_Standalone
STM32Cube_FW_F7_V1.17.1\Projects\STM32746G-Discovery\Applications\FatFs\FatFs_uSD
STM32Cube_FW_F7_V1.17.1\Projects\STM32F769I_EVAL\Applications\IAP\IAP_Main\readme.txt
STM32Cube_FW_F7_V1.17.1\Projects\STM32756G_EVAL\Applications\USB_Host\FWupgrade_Standalone
2024-11-12 2:25 PM
You have to actually write the code to make the magic happen. The ROM based System Loader doesn't provide for this mode of operation. It provides for Serial connectivity, and for USB-DFU mode
See Application Note AN2606
Perhaps look at
STM32Cube_FW_F7_V1.17.1\Projects\STM32746G-Discovery\Applications\USB_Device\DFU_Standalone
STM32Cube_FW_F7_V1.17.1\Projects\STM32746G-Discovery\Applications\FatFs\FatFs_uSD
STM32Cube_FW_F7_V1.17.1\Projects\STM32F769I_EVAL\Applications\IAP\IAP_Main\readme.txt
STM32Cube_FW_F7_V1.17.1\Projects\STM32756G_EVAL\Applications\USB_Host\FWupgrade_Standalone
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.