2020-07-09 2:52 AM
Hi I cannot connect to my Nucleo STM32F429ZI using STM32CubeIDE, the error message is:
STMicroelectronics ST-LINK GDB server. Version 5.2.3
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
Log output file: C:\Users\boubou\AppData\Local\Temp\STM32CubeProgrammer_a01060.log
ST-LINK SN : 0666FF343135485043172431
ST-LINK FW : V2J31M21
Voltage : 3.24V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x419
Device name : STM32F42xxx/F43xxx
Flash size : 63.999 MBytes
Device type : MCU
Device CPU : Cortex-M4
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a01060.srec
File : ST-LINK_GDB_server_a01060.srec
Size : 33940 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 2]
Error: failed to erase memory
Error: failed to erase memory
Encountered Error when opening C:\ST\STM32CubeIDE_1.0.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.0.0.201904021149\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Error! Failed to read target status
Debugger connection lost.
Shutting down...
Does anybody has an idea about what is wrong ?
2020-07-09 12:12 PM
And can you find that exefile at given location?
JW
2020-07-09 4:45 PM
IIRC this error occurs if you import a project from other computer where CubeIDE (or other Eclipse) is installed in different path.
The path is captured in the debug configuration and the IDE is not smart enough to fix it.
Try to delete the debug config and create new.
-- pa
2020-07-22 2:33 AM
Hello, thanks for your answers.
I don't think it comes from the exe file because it works with another card.
I tried directly to connect with the CLI. With the card that is working, the result is:
C:\ST\STM32CubeIDE_1.0.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.0.0.201904021149\tools\bin>STM32_Programmer_CLI.exe -c port=swd
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
ST-LINK SN : 066AFF363336485043072516
ST-LINK FW : V2J31M21
Voltage : 3.22V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x419
Device name : STM32F42xxx/F43xxx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M4
With the card that is not working, the result is:
C:\ST\STM32CubeIDE_1.0.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.0.0.201904021149\tools\bin>STM32_Programmer_CLI.exe -c port=swd
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
ST-LINK SN : 0666FF343135485043172431
ST-LINK FW : V2J31M21
Voltage : 3.23V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x419
Device name : STM32F42xxx/F43xxx
Flash size : 63.999 MBytes
Device type : MCU
Device CPU : Cortex-M4
=> the CLI says my STM32F429ZI has 64 MBytes flash! I am not sure it can be a software issue.
Do you think MCU is damaged?
Cedric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.