2023-06-29 7:06 AM
Hi guys,
I'm working on a Projekt, that it should be STM32F7 interfaced with a EDT-Display but without using the Operating System or TouchGFX.
The Developer had designed the Board in a way, that nobody can use it directly without FreeRTOS or TouchGFX.
I've tried to using BSP_Library but not worked. It were designed in order to work only with the internal BootLoader.
The Board which i used shown in Attachement als a Picture and its Model is : ETEMB043013XDHAL
Anybody here have an idea about that?
2023-07-04 4:59 AM
Hi @mids400
Could you please be more specific and reformulate the issue? Maybe, we can help you!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.