2012-11-11 5:36 AM
The first problem I got, was when using debugger in IAR: Fatal error: ST-Link Connection error.
Then I tried to erase flash with stm32 st-link utility, but I get an error: No STLink detected. Any idea how to fix this? The board is new and it was the first program I tried to download to it. it crashed on this programint
main(
void
)
{
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
GPIOB->MODER = (1 << 30);
GPIOB->ODR = (1 << 15);
}
#st-link-connection-error
2012-11-11 6:17 AM
Any idea how to fix this?
Get BOOT0 High and restart board, you should then be able to erase your code. Tip: Don't blind write to registers whose current content you don't know/understand.2012-11-12 5:27 AM
How do I do that? Are you talking about sb18, or the boot0 gpio pin? That one I can't get hight programatically, should I just bring some voltage on?
What's wrong with the code? I mean, it's just enabling gpios, what could go wrong here?edit:I connected boot0 to 3V and pressed reset button. The 4 leds stop blinking, but I still get ''no STLink detected''edit #2:Windows ( 8 ) device manager, shows missing driver for ST-link. But I tried instlaling both st-link_usbdriver and st-link_v2_usbdriver . But the driver is still missing.2012-11-12 8:01 AM
Driver is not signed, Windows 8 will not load unless you enable using unsigned drivers.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.