2023-08-29 2:03 AM
Hello, im wondering if it is some error in name of example, or it is work on purpose?
2023-08-29 6:39 AM
This application runs a Boost converter to output a regulated voltage at 5VDC through two selectable embedded loads.
A Voltage Mode control loop is applied to this Boost plant presuming a 2.5VDC input voltage.
Such input is obtained by halving the 5V provided by USBPD (or alternative user DC supply), through a Buck converter.
Please, note that this Buck converter is used with constant duty cycle (no control loop). It's running both a buck and a boost converter. The example is for the boost portion of this. There are other examples for the buck converter.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.