STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32vldiscovery and ST-LINK/V2

Posted on October 03, 2012 at 11:42I believe the original board only supported V1 which use the MSD SCSI transport layer for communications, where as the V2 uses direct USB end points.So is it possible to flash a STM32vldiscovery board to support ST...

OpenOCD and stlink-v2

Posted on August 28, 2012 at 09:03 I am trying to get OpenOCD to work with my STM32F4Discovery board and I get the following error: fabio@fs-1:~/workspace/stm32_code/test$ openocd -d 3 -f ./openocd.cfg Open On-Chip Debugger 0.6.0-rc1-...

usafape by Associate II
  • 9243 Views
  • 4 replies
  • 0 kudos

openocd

Posted on May 03, 2012 at 13:22 Hi all, i want to configure OpenOCD for Stlink(embedded on stm32vld board)... but after building and starting openocd i've got this output: openocd -f /usr/local/share/openocd/scripts/in...

ST link not working

Posted on October 02, 2011 at 14:29Hi everyone,I recently bought a STM32 discovery board and it seems that the ST-link is not functioning properly when I run ST-link utility it says no ST link detected, I made sure that it is in SWD mode and I have ...

rajan2 by Associate II
  • 5572 Views
  • 10 replies
  • 0 kudos

ST-Link Linux Driver

Posted on October 04, 2010 at 22:53       Is there any chance for us Linux users to get a linux kernel module to enable us to use ST-Link in Linux? A ST-Link Utility linux version would also be very practic!     #stlink #linux #openocd #st-link

Debugging STM32Discovery with OpenOCD

Posted on November 18, 2010 at 21:40Hello I've sadly got to know that native ST-Link built in my STM32Discovery won't work with OpenOCD. So my question is: what hardware would you suggest to connect Discovery with to use OpenOCD? Some Jtag? First qu...

maciekgt by Associate
  • 3212 Views
  • 7 replies
  • 0 kudos

Error initializing ST-Link device

Posted on June 20, 2012 at 22:59First post here. I have been programming the stm32f0 discovery kit for a few days now using the Atollic gdb server with no problems whatsoever, that is until today. I was in the middle of debugging and lost the link ...

timotet by Associate II
  • 2836 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.