STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problems to flash STM32H747-DISC0 board

Hi,Recently I bought two STM32H747-DISC0 boards and seems that one of them is not working properly. The first one is working well, I can flash, debug and so on. The second one, there's no way I can flash it. I tried using CubeIDE and also ST-Link uti...

0690X00000DAj1zQAD.png 0690X00000DAivcQAD.png 0690X00000DAjNRQA1.png
LPers by Associate II
  • 1347 Views
  • 2 replies
  • 0 kudos

Flash and run without debug

Here is my current approach to perform flash and run without debug:install st-link utilityin stm32cubeide open Project->Properties->C/C++ Build->Settings-> tab "Tool Settings" -> MCU Post build outputs check "Convert to Intel Hex file"Run -> Debug Co...

Upgarde Nucleo H743ZI2 to segger J-link

I have upgarded several old NUCLEO boards without any problem. All boards ware equipped with ST-LINK-V2 debugger I've tried to upgrade two new Nucleo boards board equiped wit ST-LINK-V3 .Result : Both returns error during upgrade. See attached scre...

MMagl by Associate III
  • 580 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.