2024-05-28 5:24 AM
Hello forum,
Im trying to build a function based on the BSP example and all the peripheral sensors,
when opening a new project and adding the libraries and drivers from the BSP example, nothing works.
some of the files have missing defines which suppose to come from the autogenerated files of the STM32CubeIDE
what am I doing wrong?
thanks in advance
2024-06-12 7:46 AM
Hello @ElectroManiac ,
Which libraries did you add ? Do you know what are the missing files/defines ?
Another solution is to open directly the BSP example available under Projects\B-U585I-IOT02A\Examples\BSP in the STM32Cube_FW_U5
Best Regards,
Florian LR
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.