2020-08-02 2:10 PM
After updating CubeIDE to version 1.4.0 (Linux), the debugger does not work.
A window appears
"ST-LINK firmware verification"
in which there is a message - "STLink server is required to launch the debug session".
How to fix it?
2020-08-03 3:47 AM
And I have this problem...
2020-08-06 3:21 AM
Wasted a lot of time and didn’t get results. Reinstalling the program didn’t work.
Even pre-installation of the operating system did not work. The result is the same (!!! ???).
I tried to install through the Discover program, the program does not see STLink at all, although the system sees it (lsusb) ...
I don't know what to do anymore ...
2020-08-06 1:16 PM
Same problem for me on OSX Catalina with 1.4.0 update.
2020-08-06 1:19 PM
1.4.1 is the latest and greatest version...
2020-08-06 1:44 PM
Thanks .
It doesn't show up on the update list in the IDE (yet?). I've switched to a SEGGER for now. I'll check for updates again later or manually update. Hopefully that fixes it.
2020-08-06 2:01 PM
Once you get a working version stick with it to progress on your task at hand. I was told some automotive projects refrain from upgrading once ready to start...
2020-08-06 3:07 PM
Same issue here on OSX, appeared after 1.4.0 update. stlink-server v1.3.0-4 (2020-01-29-14:18). Can we please have a fix for this?
2020-08-07 4:42 AM
I managed to install version 1.3.0. It works.
But when upgrading to 1.4.1, the problem is restored.
I will wait for the next update.
2020-08-22 11:56 AM
Update 1.4.2 is the same.:|
2020-08-22 1:01 PM
When trying to start ST-LINK_gdbserver - error
ST-LINK_gdbserver: error while loading shared libraries: libSTLinkUSBDriver.so: cannot open shared object file: No such file or directory
Should there be a folder with STLink in the plugins folder?
I have not it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.