cancel
Showing results for 
Search instead for 
Did you mean: 

Why the prefix code of NFCID2 in SENSF_RES set to '0x02, 0xFE'

diverger
Senior

In 'X-CUBE-NFC6', I found the prefix code of NFCID2 in SENSF_RES is '0x02, 0xFE'. But the IS​O 18092 says:

The 6-byte number shall be randomly generated while the prefix code is ‘01’ ‘FE’. Other settings for the prefix code are RFU.

So, what's the meaning of '0x02, 0xFE' here?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Ulysses HERNIOSUS
ST Employee

Hi,

please refer to NFC Forum Digital protocol:

Table 46: NFCID2 Format

Byte 1 Byte 2            Byte 3 – Byte 8                 Description
  01h    FEh             Dynamically Generated           NFC-DEP Protocol supported
  02h    FEh             Device Identification           Type 3 Tag Platform supported
All other values         Proprietary Identification      Type 3 Tag Platform supported

ISO18092 describes P2P based on NFC-DEP. So obviously they use 01 FE.

The X-CUBE-NFC6 example emulates an NFC Forum T3T (card specimen: FeliCa Lite-S).

Regards, Ulysses

View solution in original post

1 REPLY 1
Ulysses HERNIOSUS
ST Employee

Hi,

please refer to NFC Forum Digital protocol:

Table 46: NFCID2 Format

Byte 1 Byte 2            Byte 3 – Byte 8                 Description
  01h    FEh             Dynamically Generated           NFC-DEP Protocol supported
  02h    FEh             Device Identification           Type 3 Tag Platform supported
All other values         Proprietary Identification      Type 3 Tag Platform supported

ISO18092 describes P2P based on NFC-DEP. So obviously they use 01 FE.

The X-CUBE-NFC6 example emulates an NFC Forum T3T (card specimen: FeliCa Lite-S).

Regards, Ulysses

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.