2020-03-25 11:33 AM
Hi,
I bought new ST25RU3993-EVAL from Digikey. And download en.STSW-ST25RU001.zip on ST web site.
ST25RU3993_Reader_Suite software Installed to windows7 PC. Also installed FTDI drivers.
When i put USB cable to PC, Red LED is ON.
I see new "USB Serial Port(COM16)" on Windows Device Manager.
On the first run ST25RU3993_Reader_Suite software, automatically detect new firmware and update device with ST25RU3993_FW_v2-0-0-0_Eval.bin
Then open again ST25RU3993_Reader_Suite and click "Connect Reader" button. Then Red LED is OFF.
And software waiting and locked. No response and no any message.
I tested with different PC and Windows10, but result is same. Not working.
Why is the software not detecting the board?
Thanks.
Solved! Go to Solution.
2020-03-31 8:14 AM
Hello emre,
apparently the FW update did not pass.
Could you please force it with this procedure:
Could you please as well ensure the following bridges are duly connected:
regards,
Cedric.
2020-03-31 8:14 AM
Hello emre,
apparently the FW update did not pass.
Could you please force it with this procedure:
Could you please as well ensure the following bridges are duly connected:
regards,
Cedric.
2020-04-30 7:25 AM
hello,
after double check, only the following jumper is mandatory for correct board connection through USB:
regards,
Cedric.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.