2021-11-30 9:16 AM
There is a difference between the protocol description in the AN5512 and the embedded library package (STSW-ST25R-LIB). This seems to concern encrypted transmission.
Is 1.3.0 the latest STSW-ST25R-LIB version or is there a newer one?
Solved! Go to Solution.
2021-12-01 1:45 AM
Thank you for your message. I can see that the Application Note AN5512 contains indeed some incorrect information. For the 2 points that you have noticed, this is the STSW-ST25R-LIB that is correct. There is no encryption handled in this FTM protocol and the signification of the Bit 0 has indeed changed.
We're going to update the Application Note (it will be available on st.com in 1 or 2 weeks). In the meantime, you can get accurate information in the Annex of this User Manual: https://www.st.com/resource/en/user_manual/dm00288894-firmware-for-the-st25dvdiscovery-boards-stmicroelectronics.pdf
Here is the description of the bit 0:
b0: Bit indicating if the packet belongs to a segment.
1.3.0 is indeed the lastest version of STSW-ST25R-LIB.
Best regards
Olivier
2021-12-01 1:45 AM
Thank you for your message. I can see that the Application Note AN5512 contains indeed some incorrect information. For the 2 points that you have noticed, this is the STSW-ST25R-LIB that is correct. There is no encryption handled in this FTM protocol and the signification of the Bit 0 has indeed changed.
We're going to update the Application Note (it will be available on st.com in 1 or 2 weeks). In the meantime, you can get accurate information in the Annex of this User Manual: https://www.st.com/resource/en/user_manual/dm00288894-firmware-for-the-st25dvdiscovery-boards-stmicroelectronics.pdf
Here is the description of the bit 0:
b0: Bit indicating if the packet belongs to a segment.
1.3.0 is indeed the lastest version of STSW-ST25R-LIB.
Best regards
Olivier
2021-12-20 12:57 AM
Hi,
For your information, the Application Note AN5512 has been updated:
ST25 fast transfer mode embedded library - Application note
Best regards
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.